Schaeffler Technologies GmbH & Co. KG · Germany

 
 
Search results

Events

 
FENASUCRO & AGROCANA

2010-08-31 to 2010-09-03    Sao Paulo, Brazil

XVIII International Trade Fair of the Sugar and Alcohol Industry

ForInd NE (2nd Trade Fair for the Suppliers of the Northeast Region) and SUCRONOR (Northeast Sugar and Energy Show), that take place concurrently from April 13–15, at the Pernambuco Convention Center, in the city of Olinda, are practically sold out. Eighty percent of the available areas are sold totaling 90 exhibitors. They will find a favorable economic scenario for the region in 2010, creating great expectations.

With a forecasted GDP growth of 4.73% for the region, above the estimated average (4%) for the country, the suppliers of the industry in general and of the sugar and energy industry will have the opportunity to see this market in full growth with the start up of new plants and mills, in addition to the overhaul and modernization of existing sites.